|
The fully-automatic, crewless mass transit systems are the ideal solution for inner-urban traffic and airport links. These "people movers" are independent of the remaining traffic, ensuring fast connections and short headways by running on special rights of way. Advantages from which some of the most important cities worldwide can benefit: our automatic guideway transit systems are in use, for example, for the "people mover" airport links in Paris and Chicago, but also in large cities such as Lyons or Taipei. And in addition to the Train Control Center (TCC) further control systems also ensure the safety of the fully-automatic mass transit systems, e.g. gapless video surveillance on stations and on trains, the "automated pilots", and constant contact between the train and operations control centers - to mention but a few.
"People movers" are in successful use in the following cities:
- Germany, Dortmund
- France, Lille
- France, Lyon
- France, Paris
- France, Paris Airport
- France, Toulouse
- Taiwan, Taipei
- USA, Chicago Airport
|